{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the SFN spare doors width 700mm, compatible with NSYSFP* cabinets?
Are the SFN spare doors width 700mm below, compatible with NSYSFP* cabinets? Yes, they are.
Plain door PrismaSeT RAL9003 2000 x 700 mmNSYSFND207ED
Plain door PrismaSeT RAL7035 2000 x 700 mmNSYSFND207G
Glazed door PrismaSeT RAL9003 2000 x 700 mmNSYSFND207TED
Glazed door PrismaSeT RAL7035 2000 x 700 mmNSYSFND207TG

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.