Issue:
Maximum number of connections the BMENUA0100 module can open to the M580 CPU
Product Line:
BMENUA0100
Resolution:
The number of connections the BMENUA0100 module can open to the M580 CPU depends on the capacity of the CPU. Thus, performance of the BMENUA0100 module will depend on the time required to perform the MAST task and the selected CPU. The maximum number of connections opened by each BMENUA0100 module to the M580 CPU are as follows:

Maximum number of connections the BMENUA0100 module can open to the M580 CPU
Product Line:
BMENUA0100
Resolution:
The number of connections the BMENUA0100 module can open to the M580 CPU depends on the capacity of the CPU. Thus, performance of the BMENUA0100 module will depend on the time required to perform the MAST task and the selected CPU. The maximum number of connections opened by each BMENUA0100 module to the M580 CPU are as follows:
Released for:Schneider Electric Saudi Arabia
Issue:
Maximum number of connections the BMENUA0100 module can open to the M580 CPU
Product Line:
BMENUA0100
Resolution:
The number of connections the BMENUA0100 module can open to the M580 CPU depends on the capacity of the CPU. Thus, performance of the BMENUA0100 module will depend on the time required to perform the MAST task and the selected CPU. The maximum number of connections opened by each BMENUA0100 module to the M580 CPU are as follows:

Maximum number of connections the BMENUA0100 module can open to the M580 CPU
Product Line:
BMENUA0100
Resolution:
The number of connections the BMENUA0100 module can open to the M580 CPU depends on the capacity of the CPU. Thus, performance of the BMENUA0100 module will depend on the time required to perform the MAST task and the selected CPU. The maximum number of connections opened by each BMENUA0100 module to the M580 CPU are as follows:
Released for:Schneider Electric Saudi Arabia