{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the minimum and maximum temperature that the metallic enclosures can withstand?

Our Spacial S3D, CRN, SBM, SF and SM enclosures and cubicles as weel as the PanelSet SFN cubicles can be used under below mentioned T°:

Conditions for use: Ambient air temperature for outdoor or indoor installations: -25 to +40 ºC.

Atmospheric conditions for outdoor installations: The humidity may temporarily reach 100% at a temperature of 25 ºC.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.