{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number of jumper bar for BMXFTB2010?
Issue:
Is there a part number of jumper bar for BMXFTB2010?

Product Line:
Modicon X80

Environment:
All serial numbers

Cause:
N/A

Resolution:
The 20-pin jumper bar is not available for spare, and it is only provided for BMXFTB4000.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: