{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Secure NMC System (SNS) Tool - Unable to connect to the Cloud Licensing Server

Issue:
An error "Unable to connect to the Cloud Licensing Server" is received when using the Secure NMC System (SNS) Tool.
snstool error


Product Line:
Network Management Card 3 (NMC3) - AP9640, AP9641, AP9643

Devices with an embedded Network Management Card 3 include (but are not limited to): Metered/Switched Rack PDUs (AP71XXB, AP78XXB, AP79XXB, AP84XX, AP86XX, AP88XX, AP89XX, APDU99XX), Smart-UPS Online (SRT), Smart-UPS Ultra, Smart-UPS Modular Ultra


Cause:
When activating a Secure NMC subscription, the SNS Tool needs an internet connection to connect directly to TCP port 443 on the following server URL's:

  • https://schneider-electric.flexnetoperations.com
  • https://dsc-apps-prod.auth.eu-west-1.amazoncognito.com
  • https://www.se.com

If the network of the NMC3 enabled device is behind a proxy server, you must add a firewall rule that permits this connection and bypasses any proxy service packet inspection. Consult with your Network Administrator to configure this firewall rule.

It is also possible to upgrade the subscribed NMC via the offline method as shown below. This is an option for users on an air-gapped private network (limited to no connection to public internet). The complete instructions are also available in the SNS Tool User Guide.

SNS Tool activation

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: