{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can't I install Control Expert Diff v15.2?

The Control Expert Dif 15.2 and the HF1 can't be installed if you have already installed License Manager 2.10. This issue will be fixed in the next version.

image1

In the meantime for the new release,  the workaround is:
  • Uninstall License Manager 2.10
  • Install Control Expert Dif 15.2 and the HF1
  • Then you can upgrade the License Manager from 2.9 to 2.10, you will find the installation files on Schneider Electric Software Update.

Schneider Electric Saudi Arabia