Issue:
How to change the temperature scale of an APC Network Management Card
Product Line:
AP9619, AP9618, AP9631, AP9635, AP9635CH, AP9641, AP9643
Environment:
APC Network Management Card with environmental monitoring.
Resolution:
A customer may want to change their set temperature scare from Celsius to Fahrenheit and vice versa. This can be dependent on different factors such as policies or standards, ease of use, or just basic preference.
APC by Schneider Electric values this and takes in mind on our Network Management Cards.
You can change the temperature scale of an NMC depending on the firmware revision and/or the NMC model :
On NMC Generation 1 (AP9619, AP9618) or NMC Generation 2 (AP9631, AP9635, AP9635CH) with firmware 5.X.X, you can change this by clicking at Administration, then General, and then Preferences.
On NMC Generation 2 (AP9631, AP9635, AP9635CH) with firmware 6.X.X and above and NMC Generation 3 (AP9641, AP9643), you can change this by either selecting a LOCAL user and configuring it individually or this can be set proactively at the default user configuration settings.
Released for:Schneider Electric Saudi Arabia