{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
APC Symmetra LX (REPO) Remote Emergency Power Off Wiring Instructions

Issue:

If required, a Remote Emergency Power Off (REPO) function can be connected to the Symmetra LX. It is a critical safety feature that allows for the immediate shutdown of power to the electrical equipment in emergency situations. When wiring a Symmetra LX UPS for REPO, it's essential to adhere to all safety guidelines and local electrical codes.


Product Line:

Symmetra LX


Environment:

All serial numbers


Cause:

The purpose of this document is to provide users with a wiring guide for implementing the REPO (Remote Emergency Power Off) feature on a Symmetra LX UPS.

Note: In many locations, the Remote Emergency Power Off (REPO) switch must be installed by a licensed electrician. Refer to local and national codes. See the Symmetra LX Safety and General Information Guide or the attached file for REPO requirements and detailed safety instructions.


Resolution:

Symmetra LX REPO Guide

Schneider Electric Saudi Arabia

Attachment(s)
Symmetra LX Safety and General Information Guide.pdf [712.83 KB]