{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can't I downgrade the BMENOS0300?
This is due to a new NAND Flash hardware component introduced in Product Version (PV) 27 and greater.

If you have a BMENOS0300 that is PV27 or greater, the lowest acceptable firmware level is v1.03.The downgrade procedure will fail if you attempt to downgrade the firmware below v1.03 with a PV27 or greater.

For more information on the BMENOS0300, please visit SE.com.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: