Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Easy-UPS Online Registration
Register the Easy UPS with APC by Schneider Electric customer support. This is a one time process required to be done only during initial installation. The Easy UPS output cannot be turned on without successfully completing registration process. After successful completion of the registration process, the Easy UPS will function normally.
  1. When the Easy UPS is started up for the first time after installation, the display screen will display 3 numeric digits, “ON LINE”, “ON BATT”, “BYPASS” and “ALARM” symbols on the display get illuminated. All other symbols are not illuminated.
  2. Call APC by Schneider Electric Customer Support to obtain the 3 digit Personal Identification Number (PIN).
  3. Press the ENTER button to enter the 3 digit PIN given by APC by Schneider Electric Customer Support. When the ENTER button is pressed, all the 3 displayed digits change to ‘0’ and the first digit flashes every 1 second. Use the UP ARROW button to increment the flashing digit or the DOWN ARROW button to decrement the flashing digit till the first digit of the PIN is displayed. Press the ENTER button to accept the flashing digit and move to enter the second digit of the PIN. Repeat this process till all the 3 digits of the PIN are entered.
  4. After successful entry of the PIN, a long beep will be heard and the home screen is displayed on the Easy UPS.
  5. If the authentication of the PIN fails, then a new 3 digit number is displayed and steps 2 to 4 have to be repeated.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre