{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why my M580 SNMP service does not respond ?
----------------------------------------------------------------------------------------------------
Context
:
- All CPUs are concerned (BMEx58x0x0x)
- CPU configured with SNMP services (both IPs: IPA and IP Main)
- IP A and IP Main are not on the same subnetwork (IP A = 192.168.11.3/24 and IP Main = 192.168.10.1/24)
- but a router is only set on one of the both subnetwork (i.e. 192.168.10.254/24 )

----------------------------------------------------------------------------------------------------
Behaviour:
Randomly, on boot CPU phase, communication are starting with SNMP using IP A, SNMP services are not responding. => because router is only set for 192.168.10.x addresses.

----------------------------------------------------------------------------------------------------
Nota:
This boot phase and random behaviour are documented into "Modicon M580, Hardware Reference Guide" (ref. EIO0000001578) into chapter "Installing Modules in an M580 Rack"/"Services and Addresses"

SNMP documentation

----------------------------------------------------------------------------------------------------
Troubleshooting:
To avoid SNMP packet filtering from the router, we recommand to configure the router subnetwork mask to 255.255.0.0 (16) instead of 255.255.255.0 (24)

----------------------------------------------------------------------------------------------------
Appendix 1: Example of IP Main and IP A
IP A and IP Main example

----------------------------------------------------------------------------------------------------
Appendix 2: example of SNMP Manager
SNMP manager example

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: