Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
What is the calculation for heat dissipation in BTU/HR?

Issue: How to calculate the heat dissipation in BTU per hour Product Line: All Schneider product lines Cause: The calculation to determine the BTU for adding a piece of equipment to a cabinet to...

What is the definition of ANSI 50N/51N or 50G/51G - Earth fault?

Earth fault protection based on measured or calculated residual current values: ANSI 50N/51N: residual current calculated or measured by 3 phase current sensors ANSI 50G/51G: residual current...

What is the definition of ANSI 27R - Remanent undervoltage?

Protection used to check that remanent voltage sustained by rotating machines has been cleared before allowing the busbar supplying the machines to be re-energized, to avoid electrical and mechanical...

LINE CHOKE FOR ATV630

Altivar process has integrated DC choke (in fact 2 of them). Altivar Process is compact drive design by SE to comply the IEC61000 - 3 standard with out using any external line or DC choke. The...

Why a 4-20 mA is preferred to 0-10V in analog signals?

The bottom span 4 mA expresses a minimum signal value than a broken wire. Since the loop current never falls to zero, it can be loop powered, allowing for a two-wire circuit. 20 mA is considered an...

Are there any standards for sizing the neutral/PE bars?

The earthing schemes and sizing differ according to the earthing scheme (TT,TN-C,TN-S,IT...etc). According to the required earthing scheme, you should size your earthing and neutral conductors. IEC...

What is meant by vector group for transformers and why is it important?

What is vector group for transformers? A vector group is the International Electrotechnical Commission (IEC) method of categorizing the high voltage (HV) windings and low voltage (LV) winding...

PowerLogic PM5000 Series (PM51xx, PM53xx, PM55xx, PM56xx) Modbus Register...

Issue Register list for Modbus communication Product Line PM5110, PM5330, PM5340, PM5560, PM5563, PM56xx, PM57xx Environment Power Meter Communications Modbus Register List Cause PM5000 series...

Show more
Popular Video FAQsPopular Videos
Show more
Learn more through our Generic Knowledge FAQsGeneral Knowledge
What is meant by Symmetrical and Asymmetrical breaking currents?

issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...

What is the difference between in-sync and in-phase?

There is often confusion between the in-phase and the In-sync features of ASCO transfer switches. It is important to understand the difference between these features especially during the process of...

In a 3 phase system, why does the meter still show voltage reading on one...

Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...

Voltage, Current and Resistance Explained

Issue: How do I remember the relationship of voltage, current and resistance in an electrical system? Environment: N/A Solution: Voltage (unit of measurement - volt) is like the water pressure in the...

What is an Electrical "Ground Loop" - How does it affect my equipment?

Issue: What is an electrical "ground loop" and how does it affect my equipment? Environment: Ground loops can occur in any situation where multiple electrical devices are interconnected,...

Which RL(lead resistance from CT to relay) is to be used in Knee Voltage...

Issue: Having two different values for RL ( Lead resistance from the CT to the relay); RL from the phase CT to the relay and RL from the neutral point CT to the relay Environment: Protection Function...

Easy-UPS Online Registration

Register the Easy UPS with APC by Schneider Electric customer support. This is a one time process required to be done only during initial installation. The Easy UPS output cannot be turned on without...

What is Power Factor Correction (PFC) - Does it help conserve energy?

Issue: What is Power Factor Correction (PFC) - Does it help conserve energy? Answer: Explanation 1: Power Factor Correction (PFC) doesn't directly reduce the overall electric consumption of a...

Show more

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre