Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Ecostruxure Triconex Tricon

Triconex SIS gives superior protection for people, production, and profits

EcoStruxure Triconex Safety Instrumented Systems are an integral element of EcoStruxure Plant, our open IoT-enabled architecture for actionable business insight. With over 40 years of continuous safe operation, EcoStruxure Triconex Safety Instrumented Systems have delivered more than one billion safe operating hours.

The “one versatile system”, Tricon CX, is certified by TÜV Rheinland to safety integrity level 3 (SIL3), and can be used in all safety and critical control applications. Proven in the most demanding industries and challenging applications, EcoStruxure Triconex Safety Systems deliver a lifetime of performance.

Discover the new Tricon CX

Revolutionise process safety with Tricon CX v12
For 40 years, we have been dedicated to making the world a safer place, protecting production, people, and profits. We have taken the best of Tricon, Trident, and Tricon CX and combined them into something that will revolutionise safety and critical control.

Triconex technology platforms

Safety applications

Superior protection for people, production and profits
Reaching the next generation requires bold moves. Because realising the true potential of the fourth industrial revolution is more than digital, more than industrial internet of things (IIoT). It’s a holistic transformation to achieve the next generation of efficiency, resiliency, and sustainability.
Discover more
factory worker

Safety lifecycle expertise to maximise safety and profitability

Safety in high-hazard industries is complex and demanding. Our leading technology, software applications and dedicated safety experts are available throughout the entire safety lifecycle to ensure safety is maximised and profitability optimised.

We support your business with a comprehensive set of safety services

  • Management of functional safety
  • Define and Assess
  • Design and Implement
  • Operate and Maintain
  • Certification and Training
>Discover industrial safety services

Explore the latest insights on Triconex safety instrumented system

What is Triconex triple modular redundancy?

Triple modular redundant (TMR) architecture offers fault tolerance and error-free, uninterrupted control. The EcoStruxure Triconex includes TMR architecture for safety and reliability.

Do you need a hot spare I/O module?

Triconex I/O module is triple redundant and fault tolerant. Each module tolerates up to 2 faults without process disruption and has a 72-hour replacement window.

Why is Triconex online module replacement so easy?

EcoStruxure Triconex Safety Instrumented System (SIS) allows for modules replacement online without disruptions. Modular replacements reduce the risk of human errors in plants.

The value of inherent safety instrumented system diagnostics

EcoStruxure Triconex Safety Systems have extensive diagnostics and fault tolerance built-in. Be confident that Triconex is there continuously protecting your people, plant, and the environment.

What is “useful life” and what does it mean?

Safety controllers are assumed to have a useful lifetime of 20 years, but that does not necessarily mean your controller will fail or that you must replace your safety system as soon as that time elapses.

EcoStruxure Triconex Safety Validator in 60 seconds

Overcome the challenges of traditional manual testing with EcoStruxure Triconex Safety Validator. Take advantage of automated testing and become more efficient, accurate, and consistent.

Revolutionise process safety with Tricon CX v12

The most versatile TÜV certified safety instrumented system. One system with a choice of architectures and form factors delivering a lifetime of safe, resilient, and sustainable performance.

Tricon CX – The most versatile safety and critical control system

EcoStruxure Tricon CX enables one system for all safety and critical control applications.

Contact Sales

Start your sales enquiry online and an expert will connect with you.
Contact Sales

Process automation learning services

Explore our digital and in-person courses, specially designed to ensure the technical skills of your automation workforce are future-ready. Or request a custom learning solution to address your unique training needs.

Documents and downloads

Access offer documentation, support information, certificates, customer references, and more.

Need help?

Start here!

Find answers now. Search for a solution on your own, or connect with one of our experts.

Contact Support

Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

 opens in new window

Search FAQs

Search topic-related frequently asked questions to find answers you need.

 opens in new window

Contact Sales

Start your sales enquiry online and an expert will connect with you.

Chat

Do you have questions or need assistance? We’re here to help!

What is a safety instrumented system (SIS)? 

It is an operating system designed to automatically prevent or mitigate events in industrial processes that may be hazardous. Usually, industries use SISs in high-risk situations and tasks. That is why quite often we can see chemical processing, oil and gas, power generation, or chemical businesses make use of such a safety instrumented function. To provide a safe state and deliver reliability, these systems usually consist of three components. There are sensors that detect dangerous conditions and events in the process, logic solvers for interpreting the data sensors gather, and actuators that act to prevent or mitigate hazardous conditions. 

What are the benefits of SIS? 

First, SIS increases safety. By preventing or mitigating dangerous situations, this set of control systems protects not only people but also property and the environment. Another important thing is that SIS is highly reliable. This translates into safe operation and much shorter downtime. There will be no unplanned shutdowns. And this is a huge advantage because it enables money-saving and productivity improvements. Today’s regulations are a key element for any plant or facility. Having a system that is compliant with such safety regulations is an important benefit to consider. Interestingly, SIS can also give more confidence to operators and plant managers because of safety and reliability improvements and make the documentation process smoother and more according to international standards. 

Why the Triconex Safety Instrumented System is a solution worth recommending? 

EcoStruxure Triconex Safety Instrumented System can offer over 30 years of continuous safe operation. Furthermore, this is the leading family of high-availability and high-integrity devices that received TÜV Rheinland certification as far as safety integrity is concerned (SIL3). The highest level of protection for people, assets, and profits with continuous operation translates into reliability, low operational risk, and performance at the highest level possible.