Is the Altistart ATS48 a direct replacement for a ATS23, ATS23P, or ATS46?
Issue:
Looking for a direct replacement for the ATS48 soft start.

Product Line:
ATS23, ATS46

Environment:
All

Cause:
N/A

Resolution:
Functionally the ATS48 can replace the ATS23, ATS23P, or ATS46 softstarters.
There are some minor control and power wiring changes in certain applications.
The dimensions are not all identical. Please refer to the ATS48 User`s guide 30072-450-61 for dimensional information.


Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj