Why will the KC breakers not fit into the HCM interior?
Issue:
HCM interior cannot take KC circuit breakers

Product Line:
Panelboard, Circuit Breakers

Environment:
ILine Panelboard and Circuit Breakers

Resolution:
Size wise the KC will fit. However, the KC breaker needs a vented trim to allow the gases to escape on a high level fault. The HCM trim is not vented. But the Powerpact JJ and JL do not need the vented trim so they can be used.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj