What is the part number for the protective covers for power terminals on the ATS48 softstarters?
Issue :
ATS48 protective covers for power terminals

Product Line :
Altistart Soft start

Environment :
ATS48

Cause :
Finger protection

Resolution :
Covers are only available for the larger frame sizes of the Altistart 48.

LA9F702 - cover for ATS48C14Y and ATS48C17Y
LA9F703 - cover for ATS48C21Y, ATS48C25Y, ATS48C32Y

*Each part number has a set of 6 terminal covers.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj