Refer the below chart forair flow rate of each Altivar 32 drive.
380V / 500V 3PH | ||||||||||
Power rating | 0,37kW | 0,55/0,75kW | 1,1/1,5kW | 2,2kW | 3kW | 4kW | 5.5kW | 7.5kW | 11kW | 15kW |
Air flow m3/min | 0.24 | 0.24 | 0.24 | 0.45 | 0.45 | 0.45 | 1.32 | 1.32 | 3.2 | 3.2 |
200V 1PH | |||||
Power rating | 0,18kW | 0,37kW | 0,55/0,75kW | 1,1/1,5kW | 2,2kW |
Air flow m3/min | 0.24 | 0.24 | 0.24 | 0.45 | 0.45 |