2510KW: What is the replacement enclosure?
Issue:
What is the replacement enclosure part number for a class 2510 type KW switch?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 2510 type K Manual motor starters

Cause:
Replacement enclosure part number needed for 2510KW

Resolution:
The box only is 31056-080-51.  The cover and gasket are 31057-529-52.

Confirm the series number A or series B.  If the device is a (current) Series B, the box and cover can be replaced independently.
If the device is (older) Series A, both parts must be ordered. The B series has slightly different dimensions and the box or cover only will not fit the existing Series A product.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj