PowerChute Business Edition Backwards Compatibility for the PowerChute Server and Console.
Issue:
PowerChute Business Edition Backwards Compatibility for the PowerChute Server and Console.

NOTE: PowerChute Business Edition versions 7.x, 8.x, 9,x are no longer supported, and PowerChute Business Edition is no longer available for download from SE.com or APC.com.

Product Line:
PowerChute Business Edition (PCBE) Server and Console

Environment:
All supported OS

Cause:
Informational

Resolution:

The PowerChute Business Edition version 8.0 and 8.0.1 Console and Server manage the following old Agents:
PowerChute Business Edition 7.0.4/7.0.4a/7.0.4b Agent
PowerChute Business Edition 7.0.5 Agent

The PowerChute Business Edition version 8.5 Console and Server manage the following Agents:
PowerChute Business Edition 8.0 and 8.0.1 Agent
PowerChute Business Edition 8.5.1 Agent

The PowerChute Business Edition version 9.0.X Console and Server manage the following Agents:
PowerChute Business Edition 8.0.X Agent
PowerChute Business Edition 8.5.X Agent
PowerChute Business Edition 9.0.X Agent

The PowerChute Business Edition version 9.1 Console and Server manage the following Agents:
PowerChute Business Edition 9.0.X Agent
PowerChute Business Edition 9.1.X Agent

The PowerChute Business Edition version 9.2 Console and Server manage the following Agents:
PowerChute Business Edition 9.0.X Agent
PowerChute Business Edition 9.1.X Agent
PowerChute Business Edition 9.2.X Agent
PowerChute Business Edition 9.2.1 Agent

NOTE: PowerChute Business Edition 9.5 and above are an Agent only application. The PowerChute Business Edition Server and Console were discontinues with the release of version 9.5.
For information upgrading to PowerChute Business Edition Agent 9.5 see PowerChute Business Edition Upgrade Paths versions 9.0.3, 9.0.4, 9.1.1, or 9.2.x to Agent version 9.5

Schneider Electric Sverige

Utforska mer
Produktfamilj
Kategori:
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj
Kategori: