Can the ATV312 be powered by an external 24V only?

Issue:
Powering the ATV312 by an external 24Vdc only

Product Line:
Altivar 312

Environment:
All

Cause:
Installation/programming

Resolution:
No, this drive must have line voltage applied. The voltage must be within -15% to +10% of the rated line voltage.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Utforska mer
Produktfamilj