This error code is not documented but indicates that the Quantum 140CRP31200 module does not have a minimum firmware version of 1.56. For BMXCRA31210 with BMXNOM0200 communications on a QEIO network, the Quantum 140CRP31200 module requires at least the firmware version of 1.56.
Publicerad för:Schneider Electric Sverige