Goals and Symptoms
At what temperature do the ATS48 fans turn on and off.
Facts and Changes
ATS48 Fans heatsink temperature
Causes and Fixes
- Start for a heatsink temperature > 50°C
- Stop for a heatsink temperature < 40°C
Legacy KB System (APS) Data: RESL161689 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48