What is the difference between the SyMax 8030PS25/35 power supplies and the 8030PS25F/35F power supplies?

Issue
What is the differene between the SyMax 8030PS25/35 power supplies and the 8030PS25F/35F power supplies?

Product line
SY/MAX

Environment
8030PS25

Resolution
The PS25F and PS35F power supplies are identical in function to the PS25 and PS35 modules, except that they do not have an ON/OFF switch located on the front of the module. A separate main disconnect switch or circuit breaker must be installed to shut off power to the programmable controller system.


NOTE: The Sy/Max product line was obsoleted 12/31/2013 and the recommneded upgrade is the M580, contact your local distributor or SchneiderElectric for more information.

Schneider Electric Sverige