Conversion of a Modsoft program to a Proworx 32 project fails.

Goals and Symptoms

Conversion of a Modsoft program to a Proworx 32 project fails.

Facts and Changes

ProWORX 32 version 2.0

Causes and Fixes

Converting a Modsoft program to 'ProWORX 32' could sometimes fail and return errors during the conversion process.

This is a known issue and it will be addressed in 'ProWORX 32 version 2.1'. The converter for 'ProWORX 32'
is being completely redesigned.

As a workaround, you can use the attached ProWORX NxT converter to convert the Modsoft program to a
'ProWORX NxT' project which can then be imported into ProWORX 32.

Modosft to NxT Convert.zip

To use the 'ProWORX NxT' converter:

  • Download the attached 'Modsoft to NxT Convert.zip' file and extract all of the files to a temporary
folder on you PC.
  • Open the temporary folder and double click on the file named 'NXTCONV'
  • Select the 'Convert Modsoft database to NxT' option.
  • Browse for the Modsoft source database
  • Specify a new database name for the destination.
  • Click on the 'Start button.



Open 'ProWORX 32' and import the 'ProWORX NxT' database that was created in the step above..

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj