Issue
How to configure the STBEHC3020 for one shot.
Product Line
All versions of the Advantys Configuration Software.
Environment
Windows 7
Resolution
Wire the 'STBEHC3020' to the incremental encoder.
- Double click on the 'STBEHC3020' module to open the properties window for the module.
- Configure the parameters as shown.
- Start the PLC.
- Set the Input Validation bits to Off.
- Enable the Counter Synch
- Enable the Counter Enable
To reset the counter, toggle the counter sync bit from 0 to 1.
Publicerad för:Schneider Electric Sverige