undefined undefined
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
What is FACT (factory) protocol for ION 6200 or ION7650/7550 Meters?

Issue
What does FACt mean under protocols

Product Line
ION6200
ION7550
ION7650

Environment
Hardware protocols and specification

Resolution
Factory protocol is a terminal-like interface used at the factory for initial configuration and calibration during production. For most circumstances, this protocol should not be used once the meter is installed.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj