Our variable speed drives are designed to control three-phase motors only.
However, if the motor is replaced with a 3 phase 240V motor, a single phase 240V input inverter can be used.
e.g. ATV12 is a single phase inverter for use with three phase 230v motors.
This single phase input, three phase output function is available on the ATV12 and ATV320 drives up to the maximum rating of 2.2kw
Publicerad för:Schneider Electric Sverige