PowerLogic EM4800 Series Meter Brochure
Issue
A user requires to view specifications, features, and capability of all models within PowerLogic EM4800 Series meters.
Product Line
EM4800, EM4805, EM4833, EM4880
Environment
Feature and Capability, Comparison Table, Technical Datasheet, Brochure
Cause
A user would like to View and Compare Technical Specification of EM4800 Series meters to select the appropriate PowerLogic EM4800 Model.
Resolution
There are two attachments for the Brochure and Technical Datasheet.
See attached documents:

Schneider Electric Sverige

Bilagor
EM4800_Multi_Circuit_Energy_Meter_Brochure.pdf [1.19 MB]
PowerLogic_EM4800_Series_Technical_datasheet.pdf [1.17 MB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj