Sök bland vanliga frågor (FAQ)
Testing publication & data import in Facility Insights
ISSUE | RESOLUTION |
Following a successful publication, the ComX name has not been upgraded and devices do not appear in the Facility Insights Tree View. |
|
Usage/zone is not reported or is missing from the Consumption Per Usage widget and Consumption Per Zone |
|
There is no value shown in the Electrical Distribution widget |
|
Some widgets are missing values |
|
There is no value shown in the Baseload widget | This widget only displays values from the previous day. |
The Breaker dashboard is incomplete | Verify the breaker has been properly instrumented with the complimentary module (BSCM for compact NSX) |
There is no breaker in list of devices | Verify the box entitled is active has been enabled for the relevant breakers in the Facility Insights settings tab. |
An incorrect device has been configured in the ComX | Use the function Replace the Device in the ComX. Publish data. Data history is preserved. |
Publicerad för:Schneider Electric Sverige
Utforska mer
Produktfamilj
Utforska mer
Produktfamilj