What is the replacement for the High HP ATS01N softstarters?
Issue:
Part number for the replacement of the ATS01N High HP Soft Starters.

Product line:
ATS01, Altistart 01, High HP

Environment:
All models

Cause:
The launch of the ATS22 in 2011 caused the High HP units to become redundant.

Resolution:

The ATS01 High HP units were replaced with the ATS22 units.  These are functional replacements only.  The ATS01 had no overload protection, an internal power supply and simple dial adjustments.  The ATS22 will require external 120V or 230V power.  There are no dials to adjust, but the unit will need to be programmed.  See the ATS22 User Manual, document BBV51330 to review the wiring, dimensions and programming.  See the attached file.

ATS01N230LY - 32A rated.  Replaced by ATS22D32S6U
ATS01N244LY - 44A rated.  Replaced by ATS22D47S6U
ATS01N272LY - 72A rated.  Replaced by ATS22D75S6U
ATS01N285LY - 85A rated.  Replaced by ATS22D88S6U

Schneider Electric Sverige

Bilagor
Install BBV51330_04 ATS22.pdf [5.94 MB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj