What is the max IP of enclosure in Tricast cast resin dry type transformers?
For indoor and outdoor applications we can provide up to IP 42 in Tricast dry type transformers. Furthermore, we can increase the ingress level up to IP55 for max power rating 3150 kVA with air conditioning application and 25MVA with water cool application.

Schneider Electric Sverige