Which Modbus TCP Function Code are supported by the M241, M251, M258 and LMC058 as a Server (Slave)?The M241, M251, M258 and LMC058 accepts FC 1,2,3,4,6,8,15,16,23,43 when configured as Modbus TCP Server (Slave).
Publicerad för:Schneider Electric Sverige