How to update the variable by polling when NOP as IEC61850 client
There are two ways for the variable update in PLC when the NOP as IEC61850 client. One is polling, the other is report. Both of them need to be configured. This application present a configuration steps for the polling.

The detail of the steps can be referred the attachment.

Schneider Electric Sverige

Bilagor
AN_PAC_LCZ_NOP VariablePolling_0.1.docx [82.57 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj