Work around is the following to resolve the issue in figure 1 below:
1. Run..\Workbench\Prerequisites\VS2010ISO\English\Isolated Mode\setup.exe. When prompted, select remove
2. Run it again, this time go through the full install
3. Run Setup.exe from the root of the DVD and installation SPW
Publicerad för:Schneider Electric Sverige