Is it possible to use the same switchboard case across the ION8xxx meter series?
Issue
The compatibility of switchboard cases across the ION8xxx meter series.

Product Line
PowerLogic ION8300, ION8400, ION8500, ION8600, ION8650 meters

Environment
Advanced Revenue Metering

Cause
The user would like to use the pre-existing switchboard case when replacing the meter.

Resolution
Provided that the replacement meter and the switchboard case are of the same form factor then the two are interchangeable.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj