Firmware issue in V2.2.2 of PM5560 and PM5563
Issue
There is an issue with PM5500 firmware version V2.2.2.

Product Line
PM5500

Resolution
V2.2.2 is withdrawn from the global websites (Shopping Kiosk) due to a firmware defect. We recommend customers to upgrade their firmware to the latest version.
Use the following link for instructions on how to perform a firmware upgrade for the PM5500: index?page=content&id=FA299853

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj