Video: How do you install an option card on the Altivar ATV61 and ATV71 drives?
Issue:
Trying to install an option card on a ATV61 and ATV71 drive.

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
All

Cause:
N/A

Resolution:



Remove the front display cover by pushing down on the two tabs on the top of the drive.
Once the front cover has been removed you can now install your serial communications card or extended IO card.
Once the Option card has been installed you can not reinstall the front cover by pushing down on the cover until  you hear it click into place.

Schneider Electric Sverige

Bilagor
Option cards 1754480.pdf [670.15 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj