How to calculate source start address for MOVE block in TelePACE Studio when coil registers are copied?
Coil blocks begin at the start of a 16-bit word within the controller memory and following formula should be used: SourceAddress = 16xN+1 where N = 0, 1, 2, 3, …
Suitable addresses are 00001, 00017, 00033, and so on.

Schneider Electric Sverige