What is the Threshold at which the Altivar Process drive trips on SCF3 fault?
Issue:
SCF3 fault threshold at which the drive trips

Product Line:
ATV630, ATV650, ATV930, Altivar process

Environment:
All

Cause:
N/A

Resolution:
When the determined differential current of the three output phases is greater than
25% of the nominal inverter current, the inverter is switched off with fault message
"SCF3".

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj