Can you branch out from a variable to multiple function block input in Unity Pro?
Issue:
Can you branch out from a variable to multiple function block input in Unity Pro?

Product Line:
Unity Pro

Resolution:
Unity Pro does not allow branching out from a variable to multiple function block input pins.  A viable work around would be to use the MOVE block and the output of the MOVE can be branched out to the inputs of the function blocks.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj