Is it possible to implement Ethernet/IP explicit messaging in SoMachine?
Issue:
Implement Ethernet/IP explicit messaging in SoMachine?

Product Line:
SoMachine

Resolution:
Using the TM251MESE or the Ethernet version of the TM241 controller, with SoMachine V4.2, you can send and receive explicit messages by using function blocks EIPXM.Set_Attribute_Single and EIPXM.Get_Attribute_Single.
See attached screenshot from the help file of SoMachine.

Schneider Electric Sverige

Bilagor
Explicit.png [87.31 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj