What is the minimum value braking resistor that can be used with the ATV320 series drives?

Issue:
Min. value of the braking resistor that can be used with the ATV320

Product Line:
ATV320 series drives

Environment:
The ATV320 series drives listed below


Resolution:

db
The above information was published in the ATV320 Installation Manual dated 03/2020.
Consult the latest version of that document for any updates.
https://www.se.com/th/en/download/document/NVE41289/

Schneider Electric Sverige

Utforska mer
Produktfamilj
Utforska mer
Produktfamilj