How to install ViewX and Server Crystal Reports components

Article available in these languages: Ryska

DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as an example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.

It is commom to have to install the Crystal Reports components for both the Server and Client (ViewX) sides on an existing ClearSCADA system.
With ClearSCADA server and ViewX down, run the ClearSCADA install:


Click on "Modify":


Expand the "Server" branch:


Scroll down until you find "Crystal Reports" and select it to be installed:


Go back on the tree and expand the "ViewX Client" branch:


Select "Crystal Reports" to be installed:


Click on "Next" in order to proceed with the installation:


Click "Install":


Once the components are installed, you can create or import existing Crystal Reports objects to your application.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Utforska mer
Produktfamilj