Olika Modnet drivers i Citect, vad välja?
I Citect i hjälpen och driver help finns nedan text.
Bitordning    Lägsta coil/register nummer    Protokoll
1-16        1                MODNET (default)
1-16        0                MODNET1
0-15        1                MODNET2
0-15        0                MODNET3

If you are using a PLC that supports extended registers (6xxxxx addresses in a TSX Quantum for example)
then the following table should be used:
Bitordning    Lägsta coil/register nummer    Protokoll
1-16        1                MODNET10
1-16        0                MODNET11
0-15        1                MODNET12
0-15        0                MODNET13

Two special protocols exist for use with the TSX Quantum and TSX Premium PLC ranges.
These protocol options will select the correct addressing modes, select certain INI values and other settings to
provide compatibility with these devices without the need to set any other special parameters.
These protocols also allow you to access memory digitals and memory words using %M7 or %MW3 or %MW4.6 style addressing.
Select a protocol as follows:

PLC Model                    Protocol
TSX Quantum                    MODNET20
TSX Premium                    MODNET30

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj