Do the ATV660 / ATV960 series drives have conduit entries (knockouts) in the top of the cabinet?
Issue:
Do the ATV660 / ATV960 have conduit entries in the top of the cabinet?

Product Line:
ATV660 / ATV960 series enclosed drives.

Environment:
"Velocity" type drives up to 125HP.

Cause:
Information unclear in current literature

Resolution:
The ATV660 and 960 series drives up to 125HP have knockouts in the top and bottom of the cabinet for conduit entry, excluding the NEMA 3R rated cabinets.   The 3R rated cabinets have knockouts in the bottom only.  Input power and Motor leads can be routed in any combination of the top and bottom entries.


Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj