Video: In Citect Graphics Builder, clicking on a genie gives error "This is a static symbol...To edit the symbol, open the library and edit the symbol in the library."

Issue
In Citect Graphics Builder, clicking on a genie gives error "This is a static symbol...To edit the symbol, open the library and edit the symbol in the library."



Product Line
PowerLogic SCADA 7.x
PowerSCADA Expert 8.x

Environment
Citect Graphics Builder

Cause
Genie forms have been disabled.

Resolution
To enable forms:
1. Open Citect Graphics Builder.
2. Click Tools > Options.
3. Uncheck the "Disable genie forms"


4. Click Ok.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Utforska mer
Produktfamilj