Telepace Studio - Modbus RTU Master Programming Example
This Telepace Studio programming example will exchange data between master and slave SCADAPacks over a serial connection using the MSTR function.

These sample programs are intended to demonstrate one or more programming functions or methods and are presented as programming examples only. Schneider Electric assumes no liability for the use or application of these example programs or any portion thereof.

Schneider Electric Sverige

Bilagor
TP1 - MB_MSTR_v2.zip [11.5 KB]