Sök bland vanliga frågor (FAQ)
What are the cable characteristics to be connected to the A9XC2412 ?
Cables with the following characteristics can be connected to the A9XC2412 5 pin connector:
- The size of wires allowed is between 0,5 mm² to 1,5mm²
- wires : cooper, flexible or rigid, does not require specific performances
- The size of wires allowed is between 0,5 mm² to 1,5mm²
- wires : cooper, flexible or rigid, does not require specific performances
Publicerad för:Schneider Electric Sverige
Utforska mer
Produktfamilj
Utforska mer
Produktfamilj