Common mode filter for bearing current reductions for the ATV600 and ATV900 drives frame size five drives?
Issue:
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives

Product Line:
ATV600 and ATV900 drives frame size 6

Environment:
All

Cause:
Filter for bearing current reductions

Resolution:
The part number is VW3A5505 and its value of inductance is 183.2 uH

Schneider Electric Sverige

Bilagor
Altivar Process ATV900_VW3A5505.pdf [91.49 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj