Issue:
OLN meaning on the ATV21 and ATV212 drives.
Product Line:
Altivar ATV212
Environment:
all
Cause:
Motor overload function
Resolution:
OLN is the motor overload characteristics for self cooled, force cooled etc. The factory default is 0 for self cooled motor.
OLN meaning on the ATV21 and ATV212 drives.
Product Line:
Altivar ATV212
Environment:
all
Cause:
Motor overload function
Resolution:
OLN is the motor overload characteristics for self cooled, force cooled etc. The factory default is 0 for self cooled motor.
Publicerad för:Schneider Electric Sverige